HOMEPREVENTIONAWARENESSEDUCATIONRESOURCESREFERENCESCONTACT US
Developmental StagesInvisible ChildproofingScalding StatisticsScalding StoriesTreating Burns
Top 10 Ways To Keep Them Safe
Install a thermostatic mixing valve. The “low setting” on a hot water heater does not have a specific temperature setting, thus allowing potential Legionella bacteria growth. The thermostatic mixing valve is designed to helps prevent the need to test the temperature of your hot water heater early in the day before showers, laundry or running the dishwasher to make sure your water is at a safe temperature.  Learn More About THERMOSTATIC MIXING VALVES

Provide constant supervision for young children and those who need assistance getting in and out of the bathtub or shower.

Test the water temperature before putting children into the bathtub.

Avoid flushing toilets, running the washing machine or dishwasher when the shower is in use to avoid temperature fluctuations.

Keep hot liquids, foods and appliances away from the edge of a table, counter or stove.

When cooking on the stove, give back burners priority and keep panhandles turned toward the back.

Never drink hot beverages or eat hot foods while holding a baby. If you drink coffee or hot tea at home, use a travel mug to prevent spills and burns.

Do not use tablecloths around young children as they could be tugged on causing severe scalds from hot liquids or food.

Install proper safety devices in the shower or tub, such as handles or floor grips, to prevent any slipping or falling.  Be sure to keep the bathroom door closed when not in use.

Keep hot water bottles away from children as they have been known to burst, resulting in full-thickness burns.

_____________________________________________________________________________________
(9)Schmitt, B. (2004). Burns: prevention. Clinical Reference Systems, 502.
5How to child-proof your home. (2005). Retrieved July 21, 2005, from Consumer Watch Web site:
http://www.cbsnews.com/stories/2005/06/15/earlyshow/living/ConsumerWatch
(12)You are Never Too Young to Suffer From A Burn Injury. (2005) Santa Clara Valley Medical Center: Burn Center.
(15)Scalds: a burning issue. (n.d.). Retrieved Aug. 10, 2005, from
http://www.ameriburn.org