Instruction for re-commissioning controllers

Controllers that are already Commissioned (green dot) must be changed to Not Commissioned (blue dot) before the tool allows the controller to be commissioned again.   The follows instruction describe this process.

  1.  Existing RapidZone jobs may have all or some of the controllers in a commissioned state similar to Fig 1.  This is the Assign Neuron ID screen.

Fig 1.

 

 2.   Each controller needs to be changed to Not Commissioned from the Assign Neuron ID screen.   After completing this simple process for each controller,  the device status will be Not Commissioned per Fig 2.

Fig 2.

 

3. Use the standard Commission process to re-commission all the controllers.