|
Variable Frequency Drive Software and Energy-Savings Payback Calculator
|
Brand New Software Update - Download the most recent commissioning or loading software. Or, use the Payback Calculator to determine energy savings and payback period based on your customer's system demand schedule and variable frequency drive horsepower.
|

|
Variable Frequency Drive Software - New Revision Software Updates
SmartVFD HVAC Software
Download the software by clicking this link: SmartVFD Commissioning Tool
The Honeywell SmartVFD Commissioning Tool allows users to commission, operate, and troubleshoot their VFD from their PC. Additionally, the SmartVFD Commissioning Tool has a firmware loading tool under the tools drop down. The software works similar to the NCDrive and NCLoad tools that are available for our NX family of drives.
SmartVFD HVAC Firmware Update Process:
To upgrade to the latest version of the SmartVFD HVAC software, follow these steps:
1. Have the most recent version of the PC software SmartVFD Commissioning Tool
2. Open the SmartVFD Commissioning tool, while connected to the drive and select "online" mode.
3. Start the Launch loading Tool under Tools and load the next firmware files. The tool will ask you to
browse for the firmware file you want to download, See instructions below:
4. Verify the existing firmware is XML based (FW00778V or greater) in parameter V4.6.1. If yes, skip to step 5.
a.Download the software: XML.zip (Save the file to your hard drive, Extract the 2 files in the folder. The password is "smartsmart".
b.Via the software Loading Tool install the "Download this first to the drive.vcx". This process will take a couple of minutes, then move to step 5.
5. Download the FW0078V007.zip (Save the file to your hard drive, extract the file.) The password is "smartsmart". Install the FW0078V007.vcx file. Select the Amercas landing pack, English, Spanish, French, and Portuguese. Cycle power your VFD when complete.
SmartVFD COMPACT Firmware: SmartVFD COMPACT Firmware.zip
(The password is "Honeywell")
To upload firmware on to a SmartVFD COMPACT the MCA device is required, part number HVFDCDMCAKIT, which includes the MCA and the connection cable. Click here to see MCA instructions
Operating system software for (in zipped formats):
NXL Series drives - Version 259. Updated as of May 22nd, 2008
NXS Series drives - Version 172. Updated as of Feb. 19th, 2008
NXP Series drives - Version 174. Updated as of May 22nd, 2008
NCDrive: NCDrive - Version 2.0.11 - Updated May 22nd, 2008 (in zipped format) used for:
NCLoad: NCLoad - version 1.0.17 - Updated May 22nd, 2008 (in zipped format) used for:
-
System software upgrading
-
Expander and communication board software upgrading
-
Special application loading
-
Factory application loading
NXL Application Software (in zipped formats): ALFIQ106V205 - Version 205. Updated as of Feb. 19th, 2008
BACNet Option Card Software: OPTCJ - Version 009. Updated as of Feb. 19th, 2008
LonWorks File (in zipped format): .XIF for LonWorks
Lonbus Card software (in zipped format): .VCN for Lonbus Card (in zipped format)
VFD "Quick" Savings Estimator - click on the title (22.5kb .xls)
Annual Energy Savings Estimator for VFD's on HVAC Applications (Fans and Centrifugal Pumps)
VFD Energy-Savings/Payback Calculator - click on the title (86kb .xls)
Determines energy savings and payback period based on customer's system demand schedule and variable frequency drive horsepower.
The VFD Job Estimating & Pricing Tool is also available. Click one of the links below:
|