HOMEABOUT USPRODUCTSTRAININGNEWS & EVENTSSUPPORT & RESOURCESCONTACT USHELPVIEW QUOTE
Press ReleasesCommunicationsProduct InformationUpcoming Events
Environmental & Combustion Controls
 

Press Releases


Honeywell's New WEBs-AX Touch Screen Makes Facility Control Easier


3/30/2009



DALLAS, March 30, 2009 – Honeywell (NYSE: HON) today introduced ­­the WEBs-AX™ Touch Screen, which is expected to make monitoring and controlling facilities even easier and more efficient.


DALLAS, March 30, 2009 – Honeywell (NYSE: HON) today introduced ­­the WEBs-AX™ Touch Screen, which is expected to make monitoring and controlling facilities even easier and more efficient.

“Contractors served a critical role in the design and testing of WEBs-AX Touch Screen,” said Dave Molin, general manager, Honeywell Building Control Systems. “As a result, this device brings an unprecedented level of simplicity and flexibility to running a facility. It’s as easy to use as a quality intelligent thermostat—only it does so much more.”

WEBs-AX Touch Screen, which measures just 6” by 3.5”, interfaces seamlessly with the entire WEBs product family and readily adapts to most other standard applications.

Key features include:

·        Up to 150 configurable display screens and the ability to reference up to 150 points from one or multiple controllers networked on any data bus in the system.

·        Enables users to quickly monitor and control their site’s comfort levels, including heating, ventilation and air conditioning (HVAC) and security.

·        Configurable permission levels that limit access to system functions based on end user’s role.

·        High-definition, full-color display ideal for use in offices and other locations frequented by department managers and facility maintenance personnel. A grayscale display is available for use in HVAC rooftop units, walk-in cold rooms and similar locations.

·        Up to three data points for continuous display, giving users the ability to monitor live data, such as inside temperature, outside temperature and humidity levels.

 

Installers and technicians can use WEBs-AX Touch Screen to:

·        View system statistics, read and override system setpoints, view alarms, view point descriptions, view alarm troubleshooting notes and any other user specified data.

·        Access general device management features and information, including hardware and firmware revision levels, perform touch screen calibration, and perform flash upgrades of device firmware

For more information, call 1-800-466-3993 or visit beyondinnovation.honeywell.com.



 

Media Contact:

Sarah McHugh-Ring
Honeywell
763/954-4917
sarah.mchugh-ring@honeywell.com

 

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions.  Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.

 

 

Welcome

Login to My Account 
New User Registration

Product Search
 
 
Cross Reference Search
 
 
Search
Literature / Image Search