The new Spyder Controller 1.16 takes full advantage of NiagaraAX 3.2 with added features that support better workflow

This list represents only represent a fraction of the changes made during the upgrade of the Spyder Tool.
Download Today
Download the new Spyder Tool from the Buildings Forum for immediate use. Your local Authorized Systems Distributor (ASD) or your Commercial Honeywell Representative can also assist in providing a copy of the tool or help with any of your control needs.
Multiple Application Support
Multiple applications are now supported at every level of the programming architecture. This means that no longer does the programmer need to worry that their work will be erased by accidentally dropping an application onto an existing program. Moreover, it means that completely dissimilar applications can coexist on the same wire sheet. A VAV air handler application can exist with a boiler sequencing application. All with added flexibility to speed up programming and reduce rework.
Forcing of Individual Simulation Points
No longer do all the points in a simulation need to be forced from one screen. Now points can be forced right from the wire sheet. By allowing points to be forced from the wire sheet new points can be easily added and existing points can be quickly changed.
Full Download Support Control
Customer feedback was such that the user wanted to be able to control the type of download to the controller. The new Spyder Tool 1.16 now supports both full smart/partial downloading.
Increased Spyder Controllers per Network
We were able to take advantage of features in Niagara 3.2 that allowed us to increase the number of Spyder controllers on a WEB’s controller supporting the Spyder Tool. Testing has indicated that a WEB’s 403 controller with PVL6438N controllers running a standard VAV application was able to support over 60 controllers. This is approximately a threefold increase in the number of controllers previously supported by the same device.
Increased Download Support
Support was added to reduce failures during the download process. During download some controllers would lock up and reject new programs. The tool automatically checks for problems during download and will fix suspected controllers. This reduces install time for technicians trying to fix problems with continuous subsequent downloads.
Reduced Time for Commissioning
Field reports were identifying increased commissioning times for Spyder controllers. The tools team focused on this issue found ways to significantly reduce these times. Again this a key feature to reduce a technician’s time on a project allowing them to be more productive.